Other Parts Discussed in Thread: MSP430F149, CC1101, LM1117
各位朋友好啊,我最近在使用MSP430F149+CC1101开发无线通信。使用MSP430F149采集电压并通过CC1101发送,目前已经能够正常收发数据。
所以,我准备自己做一块板子来进一步调试。数据采集和发送端我准备做的尽可能小,准备采用3.6V纽扣电压来供电。使用型号是ER2450T,容量500mAH,正常连续工作输出电流5mA。脉冲电流大概10mA。
这个供电方案问题在于,CC1101发射状态电流大概有17mA左右,加上MSP430F149的工作电流1mA,没有使用其他外设了。这样的话,ER2450T的输出电流是不够的。所以我想给ER2450T加上3.3V稳压芯片,像LM1117稳压芯片输出电流最大能到几百mA,能够满足我的要求。但是我不确定加上稳压芯片后就能够提高我的输出电流吗?因为我的ER2450T本身输出电流才几mA。或者说有没有其他合适的供电方案呢?谢谢各位赐教啦!