与TPS56221相替换或者类似的芯片
输入电压4.5~14V
输出电流25A+
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果是必须芯片内置MOS是没有的,如果可以外部MOS,可以选择TPS51513,TPS40021,LM27402.
可以考虑simple switch电源模块 LMZ22010, 集成MOSFET和电感,支持并联和自动均流,用三颗可以输出30A,设计简单可靠性高。
如果是类似TPS56221内部集成MOS的DC/DC芯片,没有超出25A输出的电源芯片了。
所以你可以考虑上述的三芯片LMZ22010并联的方式得到30A电流。