Other Parts Discussed in Thread: LM25017
有没有小于1V的正电压转负电压的芯片
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以使用小于1V供电的升压器件将电压转为3.3V或者多少V,然后用一个电荷泵将输出电压转为负电压。这样的做法比较直接,因为本来就需要一个正电源。
如果电流不大,可以使用LM25017做一个flybuck, 副边的电压可以直接出想要的负电压。
输入电压没那么大,在3.3V左右,最好有直接将3.3V正电压转化为0.7V左右的负电压的IC;也可以将3.3V降压到0.7V,然后再正电压转负电压
具体规格不详,所以没法给出具体建议。但还是推荐一个思路给你,使用1V输入的boost电路,从SW取电作为charger
pump电路的PWM信号,用charge pump产生近似等于boost输出电压的负压。负压精度要求不高的话,可以带50mA以上负载。