This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR输出电压异常,输出电压偏高,且不稳定、FB版本不稳定

Other Parts Discussed in Thread: LM5165

用LMR10150输出3V,负载最大电流为100mA,低功耗状态为10uA,后级有无线收发模块和蓝牙SOC。SOC集成一个DCDC,作为蓝牙的供电

目前碰到问题是,

1、当接上负载之后,输出电压变成4.2V,断开负载回复正常,输出如图一所示。

2、无线收发模块每隔60S发射一次,输出电压也是每隔60S跌落到3V,但是发射时间只有1S。

3、电感封装为2520的,更换了大感值的电感也没有改善

4、增大EN的串联电阻为100K,也没反应

5、增加输出电容也没改善

电路图如下所示: