This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM1085-5.0 LM1085-12.0使用问题咨询

大家好,请问使用LM1085-12 时,输入24V,输出12V,最大负载电流为2A,是否可以长时间稳定使用;

同样,LM1085-5,输入12V,输出5V,最大负载电流为2A,是否可以长时间稳定使用;

使用需要注意哪些,谢谢!