Other Parts Discussed in Thread: UCD9244, UCD7242, UCD74120
我的设计中采用UCD9244来控制两个UCD7242,期待四个RAIL都输出动态1V的电压,可是在Fusion Digital Power Designer软件里不知道怎么配置参数,希望专家能给一份参考的UCD9244的配置文件,不胜感谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jack,
没有与你所需要的一模一样的配置,还请认真阅读UCD9244及UCD7242的相关数据手册及用户指南进行配置。对于UCD9244有一个参考配置,但是用来控制UCD74120,仅供参考。这个配置来自下面的参考方案:
十分感谢 TREVOR,终于等到回复了。。。 我现在配置了一个“UCD9244”的“XML”文件,设置的是四个通道都是输出1.0V电压,在选择CONTROL OPERATION模式,即CONTROL引脚通过FPGA拉高时会出现我附上的图1上的情况,电压输出基本为0,在我选择ALWAYS模式时,会出现我附的图2上的情况,有MRF错误,电压输出也是基本为0,我把我的配置文件也附上了,请专家帮我分析下原因啊,咋输出都是基本为0呢? 困扰好些天了,欢迎大家的讨论啊~!! 谢谢先~