This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求通过外部PWM控制电压4~5.5V输出方案 以及 LMZ31707的应用。

Other Parts Discussed in Thread: TPS62170, LMZ31707

您好!请问TI 有合适的方案可以通过PWM来动态调整输出电压吗,可调范围(3.5~5.5V)即可,精度和响应速度无要求。用于控制5V DC 风扇工作电压以降低风噪。

目前是想使用PWM经过RC滤波后接到TPS62170的FB来做,请问是否可行?或者其他更好建议?

另外我们想用LMZ31707用于消费产品降压到4.2V方案,外接12V 适配器输入。请问下从AC输入到LMZ31707的VIN通道上,需要外接什么电路吗?

谢谢!