Other Parts Discussed in Thread: GPCCHEM
上传后ti邮件回复
the following errors were reported by the calculation engine:
Error: Wrong data format, make sure file has coma or tab separated values. Name: roomtemp_rel_dis_rel.csv
文件名应该没问题,上面提到的格式是什么意思??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: GPCCHEM
上传后ti邮件回复
the following errors were reported by the calculation engine:
Error: Wrong data format, make sure file has coma or tab separated values. Name: roomtemp_rel_dis_rel.csv
文件名应该没问题,上面提到的格式是什么意思??
你好,我把数据调整了一下,现在报的错误是,请帮忙看一下,上传了新的附件
The following errors were reported by the calculation engine:
Accuracy Error: Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule
你好我调整数据后上传,现在报的错误是
The following errors were reported by the calculation engine:
Accuracy Error: Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule
请帮忙看一下,难道是因为我放电时电压下降多,软件认为不对了??附件是新的数据文件
从你的数据来看,感觉充放电的电流明显不对啊,请按照如下的步骤测试数据:
1. 设置数据采集间隔为4S,采集时间,电流,电压和温度.
2. 把电芯充饱至电流小于1C/100。
3. 静置两个小时.
4. 用0.1C的电流把电芯放电至2.9V左右。
5. 静置两到五个小时。
6. 把数据导入mathcad工具进行计算。
7. 采用多个电芯测试得到多组数据,找出最符合所有电芯的ID
你好,我用的是5300mah 3.7伏电压四节并联的锂电池,容量应该是20000mah。充电到小于1/100c,就是小于200ma应该满足了,是最终充电电流太小了吗?
0.1c放电,2000ma左右放电应该也没错啊?放到低于 2.5伏太低了吗?主要我不知道放电终止电压,我看gpcchem文档画的放到电压低于2.5伏了,这样不对吗?谢谢
其实要求就是尽可能地把电池充饱但是不能过充,你的充饱电压是接近4.3V,不确定你的电池是否是4.3V的电池,放电一般来讲放到3.0V就可以了,也有放到2.75V的。
另外,如果要做ID的话,其实没有必要一定要并联起来一起做,用单电芯来作就好了。另外需要注意一点就是电压用mV,电流用mA。
电池如果是3.7伏的,冲饱电压应该是比3.7伏稍多一点?需要先恒流再恒压,充到差不多了再涓流?例如3.9伏,4.3伏太高了吗?