Other Parts Discussed in Thread: BQ40Z50-R1, BQ34Z100-G1, ADS1203
现在我们使用的是3.7V*3的动力电池,电池成品是具有充放电、短路、过充等保护功能,现在在外部需要一个电量检测的芯片。基本电路是充电器口直接连在电池上,开关放置在负载与充电口之间,在充电的时候负载要求工作(也可以要求客户充电是禁止使用设备,但感觉不怎么好),求推荐一款芯片。 这里是不是可以用1/3电阻分压后把11.1V的电池当做3.7V的单节电池来做电量监测?控制端是ARM芯片,我看bq27441这种没有通道管理的功能,在精度要求不是太高的情况下是不是27441也可以用呢。
这里涉及的问题还有电流通道的管理,使用环境是一个脉冲电路,电流的峰值约1A,脉冲宽度500us,脉冲频率100Hz,均值电流为0.5A左右。
谢谢推荐!