Other Parts Discussed in Thread: UCC21521
最近在做一款电源,采用的是TI去年推出的UCC21521在做隔离驱动,但是在带载(输出2A,150W左右)的时候出现炸机,经过确认发现,初级的所有IC均被损坏,同时自举电路的二极管损坏,附件电路请帮忙看看是不是有什么问题,同时这个二极管在选型的时候是不是有什么需要特别需要注意的地方???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
如果你是400V做转换,或需要600V以上的管子。
Hi
这里是要快速回复二极管或者肖特基,慢管不行,同时1A电流可定不够,建议至少选5A以上。(如果你电阻选得比较小,如datasheet计算那样2.2ohm,或需要选择8A以上。)