Other Parts Discussed in Thread: TPS61196
您好,
我想知道单个TPS61196最多支持多少颗LED,单颗LED参数2.88V/65mA。
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
这款芯片最高输出120V, 假设你设置VIFB电压为0.3V, 那么每一串LED的个数为N=(120-0.3)/2.88=41.5
所以理论上总数能达到41*6=246个灯。
如果想带更加多的灯,可以芯片并联。
您好,如果输入电压是11V,理论上的总数量是多少颗? 是受最大占空比制约吗?
chen xuebin 说:您好,如果输入电压是11V,理论上的总数量是多少颗? 是受最大占空比制约吗?
你好,受最大占空比的制约,输出电压最大110V。