This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

目前正在寻找一款充电以及电池电量检测芯片 方案:BQ24610+BQ34Z100

Other Parts Discussed in Thread: BQ24610, BQ24650, BQ24600

输入电压:28V 

输入电流:<3A 

充电输出电压25.2V 即6节18650电池串联,2并6串,充电电流2A左右即可。电池 PACK包 自带电池保护板。电池电量检测以及充电部分在System端。

电池电量检测的精度控制在10%即可。由于以前的电量检测采用电压检测查表方法,但系统的带负载比较大,会突然将电池的电压下拉,故电压查表检测不准。

BQ24610的有一个功能用不到,就是当适配器输出的电关断时,不需要立即使用电池给整个系统供电。所以电路设计如下图所示:(注意充电电流以及电压等等没有具体配置电阻,所以忽略阻值等等,仅看去掉BATDRV引脚,对于其他电路有没有影响)

BQ24610 该电路设计有没有问题?

感觉BQ24600以及BQ24650 等 比BQ24610更适合自己的应用,但可能由于出货量等原因,功能强大的BQ24610更便宜点,BQ24610是否可以替代BQ24650等芯片?

除此之外,还有没有适合我的应用的  充电以及电池电量检测的方案?