Other Parts Discussed in Thread: TLV61220, TPS610987
应用场景是无线传感器,准备采用2节7号电池供电,要求电源芯片静态电流小。请问有没有推荐的芯片呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
能否具体说明一下需求,例如2节7号电池串联还是并联,输出是要3.3V还是多少? 最大负载电流又是多少?等
2节7号干电池串联,实际负载电流最大时大概30mA。输出现在还没确定,因为所选的器件包括MCU都可工作在1.8~3.6V。
进入低功耗的时候,负载电流要求在几个uA,无线收发的时候负载电流较大,大概13mA左右。
Hi
Iq较小的升压芯片TLV61220: http://www.ti.com.cn/cn/lit/ds/symlink/tlv61220.pdf
或者带负载开关的升压芯片TPS61098x系列: http://www.ti.com.cn/cn/lit/ds/symlink/tps610987.pdf
带负载开关的这种好像比较适合,但是Vsub这一路有没有电流稍微大一点的呢? datasheet里面是10mA,如果是用Vsub这一路给无线芯片供电(约13mA)就有点小了。
Hi
这个系列无论是LDO还是load switch, 电流都不止13mA, 放心用。