Other Parts Discussed in Thread: LM3409
通过LM3409 模拟调光功能 来实现LED的亮度调节。在IADJ引脚输入0~1.24V电压,可以实现电流的调节。LED的电流能够实现2mA~500mA调节。
当IADJ引脚电压为0V时,LED灯无法实现关闭(仍然有亮光,实测流过LED的电流为1.6mA),LED两端电压为7.5V。
请问怎样才能实现LED灯亮度完全关闭?(人的眼睛能察觉不到亮度),使用的LED灯条为3串29并,单颗LED灯的压降为2.8V。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM3409
通过LM3409 模拟调光功能 来实现LED的亮度调节。在IADJ引脚输入0~1.24V电压,可以实现电流的调节。LED的电流能够实现2mA~500mA调节。
当IADJ引脚电压为0V时,LED灯无法实现关闭(仍然有亮光,实测流过LED的电流为1.6mA),LED两端电压为7.5V。
请问怎样才能实现LED灯亮度完全关闭?(人的眼睛能察觉不到亮度),使用的LED灯条为3串29并,单颗LED灯的压降为2.8V。
HI
采用模拟调光时有可能因为内部运放的offset导致无法使得最小电流为零(或者说在这种情况下没有出现关断)
如果需要彻底到零,建议采用EN关断。
采用 带开关电位器(比如 WH138-1)(不能用普通的电位器),就可以实现LED亮度的完全关闭。
将开关串入EN端或者MOS管的栅极中,在配合上拉下拉电阻。