tps61021a手册中说在轻负载时进入省电模式,想请问轻负载电流是多大?省电模式时模块还能不能工作?
比如我现在想用两节1.5V的7号电池,利用tps61021a升压到3.3V为负载供电,负载最大电流100mA左右,想问下大家100mA左右算不算轻负载的情况,这种负载下tps61021a模块还能否正常工作,输出3.3V电压?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
tps61021a手册中说在轻负载时进入省电模式,想请问轻负载电流是多大?省电模式时模块还能不能工作?
比如我现在想用两节1.5V的7号电池,利用tps61021a升压到3.3V为负载供电,负载最大电流100mA左右,想问下大家100mA左右算不算轻负载的情况,这种负载下tps61021a模块还能否正常工作,输出3.3V电压?
Hi
Powersaving模式芯片同样是在工作,不同于PWM模式,在省电是pulse frequency modulation, 这个可以大幅改善轻载时的效率。
具体是从多大负载进入powersaving模式没有定义,不同芯片也存在误差,但是100mA芯片是工作在PWM模式下的。
(无论哪种模式都会正常3.3V输出的)