请教高手,我现在使用BQ25890,但是发现BQ25890寄存器已经显示在fast charging,但实际没有充电电流。
实际环境是:
直流电源接入5V,电池电压为3.35V,没有修改默认寄存器设置,读取寄存器0x0B的值为0xB7,寄存器0x00为0x48,寄存器0x04为0x20,
寄存器0x0E为0x33, 寄存器0x11为0x97,寄存器0x12为0x00.
看直流电源的电流只有0.01A。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我也遇到了,充电电流只有200mA,是寄存器设置的不对吗
Hi
测试一下电池电压,确认一下处在那个充电状态下?
如果电池电压小于2V, 充电电流是IBATSHORT. (100mA左右)
另外你可以自己对一下寄存器设置。