Other Parts Discussed in Thread: LM5161, LM5017, LM5160
现在想设计一个电源,需求是DC输入,36~60V,输出12V/0.6A,5V/0.1A,其中12V输出和输入时非隔离的,5V输出是隔离电源,共485通信用,现在想用LM5017设计,不知道这个芯片能不能满足我这个功率设计要求,LM5160和LM5161哪款可以,性价比高的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
LM5017最大只能输出600mA, 所以可以输出12V/0.6A, 但是如果再加上5V/0.1A就不够了。(除非12V电流稍微小点,将电流分给5V.)
LM5160和LM5161 电流超过1A, 都可以实现上述电压转换,两者就价格而言,TI网站显示是一样的,具体实际的价格和你们购买的量有关,量越大越便宜。(具体询价,你需要联系TI的授权代理商)