Other Parts Discussed in Thread: TPS55340, TPS61088
非常感谢您上次的解答,您推荐的TPS61088这款芯片在输入范围、工作电流电流方面符合我的要求,但是输出不够。如果我现在就用TPS55340这款芯片的话,能够实现以下要求吗?::输入范围3-6V,输出范围6-15V,输出功率达到12W(在6V-15V输出范围内的每个输出情况下,功率都能达到12W),请问能够实现吗?希望您能帮我解答,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
按照之前的计算,电流限制5.25A, 效率85%, 选择最为恶劣的情况,那么最大输出电流是 5.25/1.15*3*0.85/15=0.78A
当15V输出时,3V输入最大的输出电流只有0.78A,不够2A.
集成MOS的芯片找了一下,没有满足的,你只能找外部MOS的升压芯片。
那意思要做到输出功率12w有点勉强,那如果11W呢,可以做到吗?
Hi
0.78*15=10.7 w
10W应该是可以的。
非常感谢,还有个疑问,5.25/1.15*3*0.85/15,这个公式里的1.15和3分别代表什么意思?
Hi
电感纹波电流取输入电流的0.3倍
所以峰值电流Ip= Iin+0.3Iin/2 < 5.25A 所以可以算出Iin
3V是输入电压。
5.25/1.15*3是输入功率 0.85是效率,15V是输出电压, 计算结果就是输出电流