按照datasheet参考电路搭的LM5007 30V转12V电路给6个栅极驱动器供电,栅极驱动器未工作时,电路板工作正常,栅极驱动器收到PWM波信号,LM5007突然不工作。输入电源电压波形在关断前瞬间会出现拉低,估计是LM5007进入欠压保护,所以关断。
以前使用一颗800mA的电源芯片给同样的系统供电,使用正常,换成LM5007就出现上述情况。希望各位老师可以提供解决意见,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
按照datasheet参考电路搭的LM5007 30V转12V电路给6个栅极驱动器供电,栅极驱动器未工作时,电路板工作正常,栅极驱动器收到PWM波信号,LM5007突然不工作。输入电源电压波形在关断前瞬间会出现拉低,估计是LM5007进入欠压保护,所以关断。
以前使用一颗800mA的电源芯片给同样的系统供电,使用正常,换成LM5007就出现上述情况。希望各位老师可以提供解决意见,谢谢!
Hi
建议首先确认通过外部PPS电源供应器供电12V,确认启动瞬间以及工作状态下,最大电流是小于500mA的,原因是LM5007是500mA输出DC/DC.
输入电压被拉低, 首先确认一下输入电容Vin是否紧靠芯片Vin脚(建议稍微加大一点),其次输入走线尽量宽一点。
如果上述确认没有问题,那么再确认一下你30V电压的来源,是否有电流限制。
刚刚各种修改元器件,找到原因了,输入电容太小,导致整个系统电源质量极差,出现单片机复位、电源欠压保护等一系列问题。解决了,谢谢您。
你好,我这边遇到的问题是:输入电压36V,当输出电压大于10V时,输出电压降为2V,不带任何负载,这是为何?