Other Parts Discussed in Thread: BQ34Z110, BQ34110
有没有用ti电量计芯片做铅酸电池电量检测的,留个联系方式,交流一下?
xukai715@163.com
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以考虑BQ34Z110
DESCRIPTION
The Texas Instruments bq34z110 is a fuel gauge solution that works independently of battery series-cell
configurations, and supports Lead-Acid battery chemistries. Batteries from 4 V to 64 V can be supported through
an external voltage translation circuit that can be controlled automatically to reduce system power consumption.
The bq34z110 device provides several interface options, including an I2C slave, an HDQ slave, one or four direct
LEDs, and an Alert output pin. Additionally, the bq34z110 provides support for an external port expander for
more than four LEDs.
Hi
你用的是哪一款芯片?还是要推荐: BQ34110或者BQ34Z100-R1