Other Parts Discussed in Thread: BQ24296
用BQ24296设计电路(电路图见附件),配上电池(3.7V,2100mA),同时用电脑USB供电。SYS输出正常4.2V,取下电池或者拔掉USB,SYS的电压只有0.5V左右(同时注意到22脚REGN是低电平)。望回复,谢谢!!!
PS:电路图
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
当用USB单独供电时,你需要确认输入电流限制,这个电流是否满足sys供电需求。
当单独电池供电时,因为你的电池电压比较低3.7V以内,此时你需要注意你的SYS_min设置,有可能用3.7V电池供电没法满足这个设置,因为扣掉charge MOS的压 降,已经没有什么空间了。