首先使用LM2662输出-3.3V接2个AD8616,电压抬高为-2.2V,有人解释为AD8616 Supply voltage为5V的原因,但运放换成LMV358 Supply voltage为5.5V,LM2662输出-3.3V为-3.26V?运放是如何影响LM2662的输出电压的,如何解释不同运放压降不同呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
你需要确认负载,在接2个AD时是否有过载? 其次输入电压是否有被拉低(可以用示波器看一下输入电压。)
输入电压没有降低,始终是+3.3,输出负压随芯片改变,AD8666压降为0.3V左右。奇怪的是,今天断开印制线,飞线(LM2662与TL9721之间-3.3V引脚),串万用表测电流(3.8mA左右),此时测量电压正常(-3.2v)!实在是搞不明白为什么!
焊掉芯片,用外接电源供电,一切正常,电压不跌落,电流为4mA。现在问题很明显,芯片不能带载,一旦有电流输出,电压迅速跌落。问个问题,打NS标的2662是正品吗?