Other Parts Discussed in Thread: TPS62480, TPS54678
我需要的是一个:输入电压3~5V,输出电压范围从0~1.5V可调,最大输出电流不小于5A的稳压电源,为此我选用了TPS62480。
TPS62480的正常输出电压不小于0.6V,这是由电路结构决定的。
为了得到小于0.6V的电压,在VFB端除了正常的两个电阻(没使用RS功能)R1接输出电压、R2接地之外,增加了一个电阻R3。R3接一个可调的电压VC,调整的VC大小,就能调整稳压器的输出电压。
比如,当R1=R2=0.5R3的时候,输出电压应该是:UO=0.5*(3-VC)。
这个电路在大部分情况下工作良好,但问题是输出电压UO无法调到0,空载的时候最小只能调整到约300mV,带上0.2Ω负载之后,仍然有一个约30mV输出的电压。
现在我希望能找到另外一种芯片,能让我把输出电压调整到0V,或者带上负载之后最小电压能更接近0V(<10mV)。