This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ucc27211

Other Parts Discussed in Thread: UCC27211

用ucc27211做buck同步整流

测试一:HI,LI接地

结果:HS,HB均为11.2V左右

测试二:HI接3.3vpwm,LI接地

结果:如测试一

测试三:HI接3.3vpwm,LI接地,HS接地

结果:可以输出,但是占空比为99%的时候,输出电压为8.5v

  • Hi

       测试HB/HS是否有短路(也看chargepump电容焊接有没有问题?)

       如果没有问题,驱动HI、LI给互补的占空比看看(同步buck,一个驱动正常一个不正常是无法正常输出的)

  • 我按照你的说法做了(所有参数如图)

    电源设置:高边pwm:75kHz  3.3V  10%          底边:悬空         HO悬空

    输出结果:HB为11.2V,     HO为12V,     HS为0V,

    现把HO接上mos,输出为8V, 测试HO端口,严重失真, 过一会芯片烧毁