Other Parts Discussed in Thread: TPS61165, TPS61500
近期用TPS61165做了个恒流驱动,驱动LCD屏24V/0.2A输出,测试时发现工作一切正常,但TPS61165非常热,已经达到人手不能直接触摸的温度,非常担心长期使用折损芯片寿命,请问是什么问题导致?结构限制没有办法加散热片,若增大铺地面积会解决吗?原理图鉴附件,因做屏的背光使用,每日工作至少8小时。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
5V输入24V/0.2A输出, 效率0.85, 那么峰值输入电流是1.15* 24*0.2/0.85/5=1.3A
而这款芯片的电流限制是0.96A(MIN), 所以不建议你采用这款芯片。(实际你的电流可能不足0.2A, 而所用的芯片过流保护都是篇上限的才导致测试看起来没有问题)
其次DRV (WSON)封装热阻小很多,需要用这个封装的芯片,并加强底部PowerPad散热(铺大面积的GND)
Hi
在升压topy中, 电感纹波电流取输入电流的0.3倍,那么输入的峰值电流=输入电流+纹波电流/2= Iin+0.3*Iin/2=1.15Iin < 0.96A(电流限制最小值)
可以用封装比较大的TPS61500, 或者TPS61081: http://www.ti.com.cn/cn/lit/ds/symlink/tps61081.pdf (配置成为恒流模式, 但是误差有点大)