This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24105使用过程中发烫

您好,我在用BQ24105给12.6V的锂电池组充电的时候充电电流配置成2A芯片就会很烫,能到90多度,这种情况正常么?开关型的芯片为什么也这么烫呢?

  • 首先看一下输出波形是否稳定, 工作有无异常. 

    其次, 建议看一下PCB布线, 是否提供足够的散热区域和良好的导热能力. 建议可以参考器件手册或评估板的PCB布线. 若散热不足, 是可能造成温升过高的.

  • 我配置成1A输出的话温度就很正常,2A输出的话功能是正常的,就是发烫,PCB是两层板,芯片在顶层,底层是大面积的地,芯片中间的PAD通过过孔连到底面的。还需要其他的散热手段么?我在芯片上贴了散热片也不管用。