Other Parts Discussed in Thread: TPS62060, TPS62065
我这边用了TPS62060,1颗1.6A的DC/DC芯片
电源拓扑是3.3V转1.2V给处理器。
我们的处理器在功能模式切换时,1.2V的电流波动比较大,电流最小值是0.7A,最大值是1.1A,约有400mA的波动。
这个电流波动导致的1.2V电压波动,我们的处理器是能接受的。
但由于1.2V的电流波动,导致3.3V部分电压稳定度变差,我们的射频部分就不能接受变差的3.3V的电源稳定度。
我这边做了个实验,直接把TPS62060替换为TPS62065,结果3.3V部分电压稳定度有了明显改善。
请问:1、TPS62060和TPS62065有啥区别,手册上看不出来?
2、怎么解释用TPS62065时,3.3V的电压稳定度变好?
3、 DC/DC芯片在设计时,什么地方不一样导致输出电流能力不一样;