TPS40055的SYNC引脚接的外部555产生的250K频率,多次上电偶尔TPS40055会没电压输出,是什么原因?请问SYNC的频率和TPS40055的上电时序要那个先有?先有频率信号,TPS40055再上电吗?还是其他原因导致的?如果SYNC引脚接地,每次上电都能正常输出。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS40055的SYNC引脚接的外部555产生的250K频率,多次上电偶尔TPS40055会没电压输出,是什么原因?请问SYNC的频率和TPS40055的上电时序要那个先有?先有频率信号,TPS40055再上电吗?还是其他原因导致的?如果SYNC引脚接地,每次上电都能正常输出。
Hi
如果TPS40055启动后,SYNC再同步会有起不来的情况吗?
应该避免SYNC信号(555启动)先于TPS40055启动。
我有2路DC-DC用的是TPS40055,所以用了同步信号给这2个TPS40055,2路电路中通过1脚KFF的电阻设置了输入电压范围,一路最低输入范围是10V,另一路最低输入范围是20V,偶尔上电不输出的反而是低输入范围是10V这一路,从这一点来看反而是先有同步信号TPS40055再启动才能正常输出?
你好,请问,如果我在SYNC引脚下拉4.7K电阻到地,然后外部同步频率也接到SYNC引脚,那么上电后,TPS40055用的是内部频率还是外部频率呢?