电池为 3.7V 2000mAh,请推荐一个充电芯片,充电电流不要求,便宜即可。
另帮推荐一个放电升压芯片,要求输出5V,最大电流1A。
或者推荐一个充电和放电升压一起的芯片(如BQ24195L),这样与一个充电芯片加一个升压芯片成本不知道是否有优势呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
你具体上是怎么样的一个应用?
类似BQ24195这样的芯片即可同时充电又给系统供电(Buck电路工作),当没有输入时(buck不再充电),可以boost 升压提供5V.
BQ24195的充电和放电不能同时发生。你的应用是否正是这样?如果需要同时发生,你需要再选一个放电芯片,比如TPS61253, TPS61085. 考虑到你充电速度不作要求,你可以选一个线性充电BQ21040.