Other Parts Discussed in Thread: TPS55340, TPS61087, LMR62421, TPS61089, TPS61085
在WEBENCH上搜的TPS55340和61088/9价格有点高,结构也有点复杂,有没有成本低一点的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
在webench选型时,点击“集成电路成本” ,可以选择成本较低的方案,例如LMR62421: http://www.ti.com/lit/ds/symlink/lmr62421.pdf
2.1A开关, 如果3V电压时, 最大输出电流为3*2.1*0.84/1.15/12=0.38A
或者TPS61089, 成本也不高,同步芯片,效率会非常高,输出电流也可以做到非常大,这个芯片7A的开关电流。