Other Parts Discussed in Thread: BQ24075
手持式设备想要一颗带电源路径管理的芯片,已保证在设备工作的时候能够充满电,现在选型初步定为BQ24072,有几个问题想咨询下:
1.BQ24072 VOUT(REG)输出为VBAT+225mv,VBAT(REG)输出为4.2V
当充电电源未接,只接锂电池,此时VOUT=VBAT电压
当接上充电电源,锂电池未接,此时VOUT是什么值?是4.2V?
当接上充电电源,锂电池也接上,锂电池在充电,此时VOUT输出是多少?是VBAT+225mv?如果这样的话,那么这个时候电池的充电电压也不是4.2V了
2. 这款芯片能支持的最大充电电流为1A,有测试过当达到多少的时候芯片就比较烫,毕竟有0.8V的压降,当500ma的充电电流时就会有0.4W的损失
3. SYSOFF这个功能在BQ24075上有,主要有什么作用,哪些场合需要用到
谢谢!