Other Parts Discussed in Thread: LP2950, TPS60151
请问TPS61032PWP 5V固定输出的偏差有多大?可以推荐下输入2~4V, 输出5V的升压芯片,输出偏差在百分之一。谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
这些芯片的反馈基准误差在2%(实际分布一般会靠中心),加上反馈电阻无法1%, 所以一般输出电压在误差3%以内
1%以内的精度的芯片比较难找,请问你是什么应用?
HI
找了一下,不一定有,也不好找.TI 在芯片搜索中没有设置精度,造成寻找困难。
或者你可以将电压升起来后,再用LDO, LDO精度1%是有的。
HI
我的想法也是这样的 前端5V的用了TPS60151 后端稳压的LDO用了LP2950 不知道您是否有更好的推荐。谢谢
Hi
LDO或可以选一些高PSRR低Noise的芯片。