Other Parts Discussed in Thread: UCC2897A, TPS2373
各位TI power专家:
我目前采用UCC2897A 做一款有源正激钳位拓扑,输入 60-104V, 输出48V/10A, 主变压器采用PQ4040, Np:Ns=6:8, Lm=100UH ,次级续流电感40UH, 主要参数如电路图所示,
目前调试时,空载输出电压正常,带载50MA就不能加载了(付边电流环NC)
请教下各位专家,遇到这种情况,该如何调试,有什么好的建议,请不吝赐教。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Johnsin:
我这边也遇到同样的问题,输出只能加载30MA左右,输入是DC 36-72V,输出24V 3A(没有采用同步整流),我目前的变压器是PQ2620, Np:Ns=8:10,Lm=30Uh,输出电感47uH占空比,最大设置为0.5,现在测试Vref脚的电压5V也正常,LINEUV LINEOV的电压分别是3.6V,1.02V,另外前面的PD IC TPS2373现在是断开的,2897A的VIN脚和VDD,PVDD都有连接,请问现在是那里不合理,麻烦帮忙研究下,谢谢!