CHEM-ID选择
A电池先采用0.5C恒流,恒压taper电流小于0.01C充饱
B静置2小时
C连接EVM板,自动log DataRAM数据,间隔为4s一次
D开始用0.1C电流放电,一直放到2.8V
E静置5小时
F将以上的log的数据保存下来用MATHCAD程序计算CHEM_ID
G 通过bqCONFIG/EVSW/Gauge studio相应界面下载CHEM_ID
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,挂电子负载恒流放电即可,注意调整恒流为C/5.
我的是2s电池,选择chem id的时候,日志记录中 在bqStudio中选择的电压是Voltage(7V左右),还是Cell1 Voltage?