Other Parts Discussed in Thread: TLV62080, TPS63000
输入电压3.0~4.2,输出电压2.75~2.85V,输出恒流0.9A,使用TLV62080 芯片是否可做成此参数的降压恒流电路来驱动LED呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
不能,原因是FB有0.45V, 加上LED 2.85V, 使得输出为3.3V,即便100% duty,输入也需要3.3V, 而实际建议在3.5以上。
满足这个条件就可以了。
请问:输入电压3.0~4.2V,输出电压2.75~2.85V,输出恒流0.9A,使用TPS63000 芯片是否可以实现呢.