Other Parts Discussed in Thread: TPS63002, TPS55010, SN6501, TPS732
你好:
我用tps63002做了一个5V稳压,问题有两个:1.功耗有点高,5V50毫安的输入带不动,芯片发热。2.我在输出端提供5V电压,在输入端有1.5V电压,我希望能做隔离,在输出端提供5V电压,输入端为0,以此判断正反插。可是这样不行。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,输出5V时输入也是5V,我就是输出的电流不大,电感饱和电流足够,我就是想做一个隔离,能正向流过电流,反向不能流过(我的要求是能达到:输出端接5V,此时输入端无电压,并且正向输入时无压降和低功耗,)。
Hi
TPS63002最小输入时1.8V,输入偏低是会带不起来,注意采用Powersaving模式。
这个芯片在关断(不启动)时输入和输出是断开的。
如果选择隔离芯片,可选择TPS55010: http://www.ti.com.cn/cn/lit/ds/symlink/tps55010.pdf
输入是有5V的,是被拉低了。另外,还有没有比TPS55010小的封装的,以及外围器件要少一些的?
HI
芯片内部击穿导致的,芯片已损坏。 你需要确认电感是否有质量问题,饱和电流必须足够。
SN6501也不错: http://www.ti.com.cn/cn/lit/ds/symlink/sn6501.pdf
我刚刚看了一下,TPS732这个封装还行,外围器件少,输出电流250也足够,不知道能不能满足隔离的要求?
还有没有其他方案啊,要小封装,越简单越好?哪怕是一个无压降的二极管,正向导通,反向截止就可以,能过300MA电流就行。谢谢!