This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS259230 输出关断时候输入电压抖动

Other Parts Discussed in Thread: TPS259230-41EVM, TPS25923

你好,有客户在测试TPS259230这个EFUSE功能时候,发现在关断输出瞬间,输入电压抖动,请帮忙分析原因,谢谢

在TPS259230-41EVM样板上,使用TPS259230测试时,发现以下现象

 现象:使用样板上TPS259230的电路测试5V功能,在2A负载的情况下,将IC的开关S1(EN信号)拉低,测试发现5V VIN电压在5V OUT电压掉电时出现振荡。

              5V VIN振荡时最大值电压达到5.98V,测试波形见图一。

  • Hi

       从datasheet测试的波形看病没有在关闭时有这个震荡。

       请问5V输入是什么(开关电源还是设备输入的)?  输入源到芯片TPS25923芯片的输入是否存在较长导线(线路)?

  • 这个应该是5V输入引线过长造成的,切断输出,输入导线上的分布电感储存的能量无处释放,产生的震荡,可以考虑以下方式解决

    1、缩短引线距离

    2、在5V输入加一个相对较大的电容。