Other Parts Discussed in Thread: UCC28250, TL594
用于充电器设计如何选择?
超级电容充电器
输入 AC 220V 50HZ 输出DC250V 3A 800w。为超级电容充电。
超级电容是:
超级电容单节:2.7V 350F ,一组:单节*6=16V,一串:16V*15组(串联)=240V.
请教下采用哪种方式来实现?双管正激?BOOST?
采用何种IC? UCC28250? TL594?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.