Other Parts Discussed in Thread: TPS2556, TPS2557, TPS2559
问个问题,用了TI的方案做一个限流3A的USB充电方案,请问:
1、满足需求的情况下,TI的哪款芯片价格最便宜。
2、TPS2556,2557,2559芯片更推荐哪款芯片,原因是啥。
3、能否提供上述推荐芯片的参考设计。
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
TPS2556/TPS2557的主要差别是使能电平控制逻辑:
TPS2556: EN pin is active low.
TPS2557: EN pin is active high
TPS2559性能要好一些,跟高精度的电流限制,更低的导通电阻,更高的使用温度等。
符合要求选择哪一款都是可以的,你需要根据你的设计要求选。 例如你要选择成本稍微低一点,选择前两者。 如果使用时要求最高温度超过85摄氏度,就选择后者。
你好,能否提供具体的参考电路设计,谢谢!
或者能否提供贵司技术支持的联系方式,谢谢。
你可以使用WEBENCH软件自行设计,里面有原理图和仿真结果以及Layout
你好。顺便问一下,2559是恒流输出的,那么Datasheet里面的热关断模式是什么意思,能够保证过流的时候,电流一直限定在3A输出么。
Hi:
datasheet上有描述:
The TPS255x responds to overcurrent conditions by limiting their output current to IOS. When an overcurrent condition is detected, the device maintains a constant output current and the output voltage reduces accordingly. Two possible overload conditions can occur.
The TPS255s thermal cycles if an overload condition is present long enough to activate thermal limiting in any of the above cases. The device turns off when the junction temperature exceeds 135°C (minimum) while in current limit. The device remains off until the junction temperature cools 20°C (typical) and then restarts. The TPS255x cycles on and off until the overload is removed
如果持续过载,芯片温度上升到热保护,芯片会关断。 所以过载虽然恒流没有问题,但是一旦过温,芯片是会保护掉的(关掉)
你好,这个芯片的设计可以参考用户手册:http://www.ti.com.cn/cn/lit/ug/sluub15/sluub15.pdf
关于Fault可以控制EN,具体设计参见Datasheet的Figure18