您好!关于tps40090,我的应用条件是:
1、输入电压1600V~1900V
输出电压640V,输出电流600A
四路buck电路降压
设定工作频率1.5kHz
2、问题是:在我做好相应的隔离、放大等外围电路后TPS40090能否应用于上述工作条件;1.5kHz的工作频率该芯片是否可以做到?
谢谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!关于tps40090,我的应用条件是:
1、输入电压1600V~1900V
输出电压640V,输出电流600A
四路buck电路降压
设定工作频率1.5kHz
2、问题是:在我做好相应的隔离、放大等外围电路后TPS40090能否应用于上述工作条件;1.5kHz的工作频率该芯片是否可以做到?
谢谢!!!
芯片手册给出最低工作频率为100kHz,不适合工作在1.5k这么低工作频率。 不知道您这是一个什么样的应用?为什么会选择这么低的工作频率?有什么特殊的要求吗?
这是用于地铁的能量回收的,TPS40090的交错控制方式刚好符合我的设计要求。该项目总功率260kW,四路交错并联,每路功率是65KW,用IGBT作开关器件,因此频率不能做高。类似TPS40090这样工作方式的芯片那种的开关频率可以到1.5kHz,或者是多片联立的那种也行,请推荐!
HI
这么大功率,用多相DC/DC+IGBT,也都是需要额外增加专门的IGBT芯片。而大部分芯片DC/DC频率都没有办法做得这么低,即便采用外灌,也不一定好控制。