Other Parts Discussed in Thread: TPS61230, TPS62130
你好,我在使用TPS61230遇到一些小问题,输入电压3.7V输出电压5V但是输出的电流只有500mA左右,请问这是什么引起的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,布线是按照datasheet,器件选择上同手册推荐的电感,容值匹配相同,实测负载能力650mA,电感饱和电流这个怎么选择?
Hi
效率明显低了,这个有问题,建议确认电感。芯片看起来没有问题,电感将是最可疑的功率消耗器件。
换一个以前用过的电感,饱和电流2以上。 带载超过1A不会有问题。( 按照1A输出, 5V*1A /0.9/3.7V*1.2=1.8A)