This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61021A升压模块带负载能力

Other Parts Discussed in Thread: TPS61021A

请问输入1.8~3.2V,输出3.3V的TPS61021A典型电路可带动最大多少安培的负载?若负载正常工作最大160mA,TPS61021A能否带动正常工作,输出3.3V?


  • Hi  

        最大负载能力与输入电压曲线图如下:

        

       红线是3.3V输出,从曲线上看最大输出电流在1.5A以上。

     (但是这个曲线可能不是按照最小3A的电流限制的结果算出来的,实际建议带载不要超过1.2A。 如果你只是要带200mA以内负载,绝对没有问题。 Layout上注意你需要注意必须有足够的输入电容尽量靠近电感输入端,其次电感的饱和电流需要足够大)