Other Parts Discussed in Thread: TPS65217, TL5209
公司产品是在BeagleBone-Black基础上做的,加上了锂电池,想实现shutdown -h 关机时断掉所有电源,但是每次关机后TPS65217C的LDO2总是还有电压输出,加了个400欧电阻试了试,关机后还是有1.175V 的电压,不知道这个是什么情况,如何解决这个问题,请教技术支持。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LDO2即使有输出也应该是3.3V左右,现在输出1.175V也不对。你LDO2有挂负载么?正常工作时,LDO2输出是多少?
方便上传一下你的原理图么?
感谢你的回复。
今天上班来了打算好好测试一下,然后总结一下情况发给你,但是测试时发现关机后LDO2和LDO4同时都还在输出1.175V,而且LDO4接了一个10uF的电容,于是并了个510欧的电阻上去,发现执行shutdown -h now 指令后能实现断电了,LDO2和LDO4都是0V了。
我们的硬件,核心板用的是beaglebone-black,自己做的底板,看核心板原理图上TPS65217外部LDO2和LDO4并没有什么联系,但是貌似关机后LDO2是跟随LDO4输出的,这个问题还在考虑。。。
现在新的问题是要是加着5V外电再执行关机,完成后LDO2和LDO4还是总有2.2V的输出,这个可能是beaglebone-black硬件上有什么联系还没分析。
看手册上LDO4有个负载开关的功能,这个是不是跟上面出现的情况有关系呢,关于LDO2和LDO4的内部联系,或者执行关机时LDOx的正确操作流程,希望能得到明确的指点。。。
我打算把beaglebone-black的原理图传上来,貌似格式不对。。。
贴图吧:
对于PWR_EN管脚,其拉低时,芯片会进入两种模式OFF 或 SLEEP mode,而两种模式的区别是sleep模式下,只有LDO1是不会被关断,其他电源轨都会关断,所以我估计应该是你后级的问题,建议现将LDO2和LDO4 的负载断开,只接电容,看芯片disable时是否有输出
恩,也怀疑过跟负载有关,但是LDO2的输出都在这个块原理图上,从图上能看出来它只接了一个LED灯一个2.2uF电容,还有就是那个TL5209的使能引脚,貌似负载影响它的几率不太大,而且还有个问题就是,LDO4和LDO2貌似互相有影响,两个都接下拉就没事,任何一个不接下拉电阻,另外一个就不会彻底断掉,而且两个输出的电压是一样的,一个是2.2V另一个也是2.2V,不过现在能正常断电了,先这样用着,等以后我们自己做核心板时肯定还得面对这个问题,周期比较紧张,我们先往下进行了,谢谢您的帮助。