我们使用BQ24630给4节索尼的磷酸铁锂电池充电,产品用于野外,目前遇到在野外挂机测试,遇到电池电被放完,再次充电发现BQ24630不能充电,更换电池后能正常充电。请问大概是什么原因不能充电,有没有方式可以实现给这种放完电的电池还能充电?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们使用BQ24630给4节索尼的磷酸铁锂电池充电,产品用于野外,目前遇到在野外挂机测试,遇到电池电被放完,再次充电发现BQ24630不能充电,更换电池后能正常充电。请问大概是什么原因不能充电,有没有方式可以实现给这种放完电的电池还能充电?
电池供应商说是可以放到0V,附件是电池的规格书。
1.再次充电不能充电的判断依据是什么?有没有可能是充电电流太小(仅为125mA), 充电速度慢,造成判断错误。
2. 此时正常应该为125mA的pre-charge电流,注意电池在极端低压可能有内阻极大的情况,如果125mA*R_battery太大,会造成输出过压。
3. If the VLOWV threshold is not reached within 30 minutes of initiating precharge, the charger turns off and a FAULT is indicated on the
status pins. 如果30分钟,电池电压不能充高到一定程度,就会关断充电。