Other Parts Discussed in Thread: TPS61500
输入能力5V 2A (移动电源供电)
LED 2串以上(无论几串,最终总功率6W,比如2串LED压降6V,那电流1A,总功率6W)
要求效率尽量高,最好能在90%以上,另外如果保证输出6W功率的情况下几串效率最高?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS61500
输入能力5V 2A (移动电源供电)
LED 2串以上(无论几串,最终总功率6W,比如2串LED压降6V,那电流1A,总功率6W)
要求效率尽量高,最好能在90%以上,另外如果保证输出6W功率的情况下几串效率最高?
HI
如果是要生压,可以采用多个LED串联(不需要并联),但是不建议串很多,否则效率会降低。
如果是这样你可以选择TPS61500.
( 如果希望效率尽量高,建议用降压的topy,不需要LED并联,采用高亮度的LED。)
可以采用多个LED串联(不需要并联)
这里强调“不需要并联” 是并联会影响效率还是什么?
比如4串和4串N并
Hi
采用并联是你需要考虑各串电流是否平衡(一样)。
Hi
这个你可以在调试中确认,可选择500~700kHz。