Other Parts Discussed in Thread: TPS61195, TPS61199
112个3-3.2v,20mA,led灯,原来用过的tps61195是否能带这么多灯?不行的话有什么别的方案,望老师指点!谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi JianHua:
使用TPS61195, 推荐的最大输出电压时45V, 按照您的参数Vf=3.2V, 14灯串,输出电压降达到44.8V, 勉强可以,如果是这样的话,可以改为13灯串,然后增加灯的亮度来达到亮度的设计需求。
否者您可以采用TI的TPS61199, 它并非像TPS61195 MOS集成于芯片内,而是采用MOS外置,输出电压可以做的比较高,FB脚电流可高达70mA, 可满足您12V usb供电的设计。(这个芯片输入电压范围是8~30V).