This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用TPS61040时,电感、输出电容出现啸叫现象

Other Parts Discussed in Thread: TPS61040

现使用TPS61040过程中会出现电感电容啸叫的问题。

我输入的电容为一个100uF的电解容加106瓷介容,而输出电容则是一个50V的10uF电解容外加一个475瓷介容。而电感则是使用一个10uH的工式电感。

我通过主芯片输出的PWM(770Hz)来控制TPS61040的使能脚,并改变占空比从而实现调整背光亮度的功能。当占空比最低时,此时液晶背光亮度最暗,电感和电容也叫的最厉害。

想询问各位是否有遇到类似的问题,是如何解决的?

另外一个就是,前馈电容CFF是如何实现降低纹波的作用的,怎么去分析?

  • Hi  

       引起电感电容啸叫的原因可能是电解电容引起的,电解电容并不适合应用于高频率的电源转换中,建议您将输出电容改用低ESR的1uF的陶瓷电容或者2个1uF的陶瓷电容并联也可(更低ESR).

       输入电容10uF已经足够,可以采用2个4.7uF的陶瓷电容达到更低纹波的效果。

     关于前馈电容,见datasheet描述: A feedforward capacitor across the upper feedback resistor R1 is required to provide sufficient overdrive for the error comparator. Without a feedforward capacitor, or one whose value is too small, the TPS61040/41 shows double pulses or a pulse burst instead of single pulses at the switch node (SW), causing higher output voltage ripple.

  • 建议你使用TI的仿真软件仿真,有助于你看看你参数是否合理

    仿真软件中就有这个TPS61040的库

  • re: Johnsin Tao

    楼主说过: 输入的电容为一个100uF的电解容加106瓷介容,而输出电容则是一个50V的10uF电解容外加一个475瓷介容.

    在高频条件下,那怕100uF和10uF的电解都不起作用,106(10uF)和475(4.7uF)也足够了。

    ESR不是越小越好,要看系统环路参数配合

  • 人耳朵听到的频率都低于20KHZ,所以,你调光的PWM信号提高到900K试试看,另外,环路补偿加RC试试看。FB脚有没有收到干扰等,PCBlayout 也要这些检查下,避开干扰源。FB脚。

  • 我主芯片的PWM只有97Hz、194Hz、388Hz、776Hz这样几个固定的频率,无法再上去了。

  • 今天有对输入的电流进行测试,在我最初提的这个条件下,纹波电流波形如下:

    由于我的PWM是控制芯片的使能脚,频率是194Hz,此时的电流波形就是这样的,占空比为14/32,这时候这时候就电感在啸叫。

    我在想说是不是我后面的电容过大导致的出现这样的震荡的电流信号。所以我就把肖特基二极管后面的电容全部去除,贴一个0805的村田1uF瓷介容,重新上电后,该瓷介容也开始啸叫,而且更加大声。

  • Hi

        TPS61040 内置MOS的电流限流是350~450mA, 按照datasheet: http://www.ti.com.cn/cn/lit/ds/symlink/tps61040.pdf,最大峰值应留应该不足500mA,从你测试的电流波形看,芯片会受到限流保护。通常造成这种情况的原因是电感饱和,请确认您10uH的电感,饱和电流是否超出500mA(通常极性电容接反也会造成这种效果,但是陶瓷电容没有极性,所以建议先确认电感).  而对于一般20mA的LED输出的设计,输入电流也不会到达这么大,datasheet 第十六页有典型应用图。

     另外电解电容确实不适合这里的应用,适当的采用低ESR电容时可以降低纹波的。

     可以的话,更加详细的说明您的测试,输入电压,输出电压,输出电流等,可进行进一步的确认。