Other Parts Discussed in Thread: TPS62130A, TPS63027
输入端:18650两节并联,提供2.8V-4.2V 7A的输入源。
负载端:单颗LED,工作电压3.3V - 4.3V 电流1A - 3A,呈线性。
有没有这样的恒流源芯片,PWM可控制电流大小,然后在电池3V的时候可以提供给负载4V的电压,电池在4V的时候可以提供给负载3.5V的电压。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
非常感谢,我看到这款芯片Switch Current Limit (Typ) (A) 是4.5A,Iout (Max) (A) 是2A,输出电压是1-5V,能否给解释一下,4.5A 2A分别是哪个说明情况下的电流?我的负载是线性的,从3V到4.3V,我有个疑问电池电压等于4V的时候,如果负载需要4V 2.5A的电流和电压,是不是没有任何一款芯片可以这样?如果确实这样,那这个方案就不能这么做了。