Other Parts Discussed in Thread: TIDA-01093
目前准备做一个低速车的BMS,成本要求很高,目前在评估TI的参考设计,TIDA-01093。但有些疑问请教下:
(1)芯片供电电压VBAT比VC10电压小0.7V以上,对采样精度有无影响?
(2)芯片供电电压VBAT比VC10电压小0.7V以上,对采样精度有无影响?(VC5X_U得电后即打开开关)
(3)D48这样接的目的? VC5与VC5X,VC10与VC10X(76940)之间什么关系?
(4)I2C使能控制(电源控制)逻辑?
(5)TS1这样控制设计的目的? 3.0M下拉电阻(R126)是否为必须?为什么? TS1/TS2温度采样内部是否已有上拉? TS1/TS2输入是否有必要加LPF滤波和稳压二极管?
(6)芯片是否有采样输入断线诊断功能
(7)在芯片正常供电情况下, 输入0~2V范围能否检测t5r?
(8)76930的BAT与VC5x,VC5x与VSS之间是否需要加稳压二极管
(9)C15与C20之间这样处理的目的?
(10)芯片诊断/保护、Pack电压计算、休眠/唤醒等功能