This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650充电半小时后,充电异常(STAT1和STAT2均为OFF)问题咨询求解答

Other Parts Discussed in Thread: BQ24650

各位大神好,我用TI芯片给铅酸电池充电,目前已经做了5块样品,发现问题如下:

BQ24650的输入电压在12V,给电池输出充电的输出电压为6.8V(实测电压为6V左右),刚开始充电是没有问题的,但是充电半小时以后,发现STAT1和STAT2引脚输出为高,导致LED熄灭(即充电故障),此时测量BQ24650的PH引脚无电流输出(用万用表测量R26两端的电压为0),无法实现充电。5块样品我分别测试了好几次,都会出现这个问题,麻烦各位大神帮忙看一下是什么原因?多谢~

备注:

1、原理图见附件

2、原理图中R26标注的为20mΩ,我实际样品贴片时,R26焊接的是45mΩ